Issue
Some system administrators wish to set up very limited privileges for certain users but need those same users to be able to do a controller reload. What are the minimum user security "keys" required to set this up?
Environment
Continuum CyberStation
Cause
Incorrect user security settings (locks vs. keys) will not allow a logged on user to reload a controller.
Resolution
In order for a limited user to be able to reload a controller, that user must have user security settings to reset, teach, create, and edit (if applicable) every item inside that particular controller (i.e., InfinityNumerics, Infinity Inputs, schedules, groups, etc.) as well as the same privileges for controller object itself. See also the CyberStation Online Help System under Security Editor topic.