Issue
When adding an additional WS to an existing SU(SingleUser) SQLExpress PC, DBInit -> Workstation Configuration gets error message "SQL Server PC_Name does not exist or access denied. Workstation Setup Failed! Please try again or click Cancel to exit."
Environment
Continuum Cyberstation version 1.82 and higher with MS SQL Express.
Cause
MS SQL Express requires Instance Name as SQLExpress for Database connection.
Resolution
Set value of the Server Name in Workstation Configuration of DBInit to "SU_PC_Name\SQLExpress".
For example, if the computer name of the existing SU Workstation is "MyPC01", you need to type "MyPC01\SQLExpress" in the Server Name attribute of the Workstation Configuration of the additional Cyberstation.
Note: A SU SQL Express database can only support up to 2 additional Workstations.