Issue
Running SevenReports a C++ Run Time error. Happens either in Archive data reports or database reports
yyyy-mm-dd hh:mm:ss
Environment
I/NET Seven version 2.16 to current
Cause
Scope of Data yyyy-mm-dd hh:mm:ss
Resolution
Run the archive file SevenReport or ArchiveSevenReport file with the following steps in mind
1. If using Archived reports, mount the archive file with the desired dates to search
2. when the date range comes up on the screen, offering to search with date, hour, minutes, and seconds yyyy-mm-dd hh:mm:ss limit the time range. The whole key here is to limit the time range. Example of range is below.
The crash was due to the report program attempting to generate a report with to much data to sort through. Be patient. Even on old computers, with XP, 500MB or RAM, and limited resources, the reports will be produced.
Time and time again, this issue comes across. Using my old computer in the lab, the database from the customer is loaded, the archive files are loaded and still it works every time. The C++ Run Time error appears when expanding the search to more data and crashed the report. But limiting the amount of time to minutes or perhaps one hour, produces a report. (For an example of unusual examples: there have been 2 minutes of time for the search criteria, and 38,000 pages of report produced.)