BACnet Protocol Implementation Conformance Statement or PICS for Niagara R2 and Niagara G3

Issue

Trying to locate the BACnet PICS for a UNC and ENC.  Where are they located?

Product Line

TAC I/A Series

Environment

Niagara R2 revision 522 and higher

Niagara G3 revision 3.2 and higher

Cause

Trying to locate a web-based resource for this information

Resolution

For Niagara R2, click here for the BACnet PICS.  Updates to this document are available via the iPortal website ( http://usiportal.tac.com ).  Request an account and check the Links drop-down menu for the 'Publication Zone'.  Do an advanced search for document F-27462.

For Niagara G3, click here for the BACnet PICS.  Updates to this document are available via the iPortal website ( http://usiportal.tac.com ).  Request an account and check the Links drop-down menu for the 'Publication Zone'.  Do an advanced search for document F-27463.