Issue
Vista IV Remote Workstation pulling the Workstation license from the server PC shows the error "The object involved has disconnected from its clients." If the alarm is acknowledged, Remote Workstation does not work. Restarting the Remote Workstation restores functionality.
Environment
- Vista IV Remote Workstation
- Aladdin Privilege Administrator 2.01
- Remote license hosting
Cause
The Aladdin Privilege Administrator 2.01 licensing tool that comes with Vista IV did not handle remote licensing of Workstation very well. If trying to read the Workstation license from the server at the remote PC, it occasionally will time out and result in this error.
Resolution
Install a Workstation license/dongle on the remote PC. This will prevent it from trying to read a license from the server PC and resolve the issue.