Issue
Trying to find all BACnet devices under a bCX by right clicking the device in the Continuum Explorer and selecting 'Find BACnet Device', no error is received but no devices are found even though there are BACnet devices on the bCX's MSTP port.
Furthermore, a Wireshark capture shows who-Is message was qualified with bCX's device id.
(example, who-Is, 2587214-2587214)
Environment
Cyberstation
bCX4040
b3s
Cause
When a 'Find BACnet Device' is issued from a specific bCX device, Cyberstation direct the who-Is message to the particular device.
Resolution
To find all BACnet devices right click the root folder and select 'Find BACnet Device' from the root.