Issue
What issues, if any, are there to replacing Workplace Tech 5.7.7 with 5.7.6 on a Windows XP computer?
Environment
Workplace Tech 5.7.7 and 5.7.6
Cause
none
Resolution
Workplace Tech version 5.7.7 comes with new firmware for the MNB-1000. It is better to use version 5.7.7 with any MNB-1000 controllers installed with the new firmware. This is especially true on job sites adhering to GSA guidelines.
If the computer is only used with MNB-1000 controllers running previous firmware releases, then re-installing version 5.7.6 won't create any issues.
Review the release notes below for more details.