Issue
The application requires use of an object that only exists in newer versions of the programLib jar file.
Environment
I/A Series R2 (all versions)
Cause
Requires use of objects only available in newer versions of the programLib jar file.
Resolution
There have been no schema changes to the programLib jar file that allows the jar to be installed and used with previous versions of I/A Series R2. Download and install the latest programLib jar file version from The Exchange Download Center.