Issue
Can a Niagara R2 Enterprise Server and Niagara G3 Enterprise Network Server be installed on the same computer?
Environment
Niagara R2 all versions
Niagara G3 all versions
Cause
None
Resolution
The Niagara R2 ES software and Niagara G3 software can be installed on the same computer provided the following:
- The Windows operating system is supported by both platforms (e.g. Windows XP)
- Only one Niagara service can run at anytime (so both platforms cannot run simultaneously)