Issue
Some actions selected in the event notification repeat each time an alarm is repeated and others do not
Environment
Continuum
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Some actions can be repeated when using repeat alarms and others are not
Resolution
Actions that will repeat are:
Display alarm view- time stamp may be the only change
Display Graphic
Run Program
Display Video
All these items are listed in the points alarm tab with specific object links at the bottom
Actions that will NOT repeat are:
pages
beep
blink
etc