Issue
When attempting to Discover devices on the Niagara Network getting the following message: java.net.socketException can't assign requested address.
Environment
G3 (Niagara) ENC
Cause
The address in the default gateway of the ENC is invalid.
Resolution
Under the station Platform open TCP/IP Configuration and enter the proper gateway address in the "IPv4 Gateway" field.