WorkPlace Tech revision 5.7.7 installed on a Windows Server 2003, 64-bit machine: Error initializing the dispatcher for WorkPlace Tech. WorkPlace Tech may need to be reinstalled in order for the dispatcher to function properly.

Issue

WorkPlace Tech revision 5.7.7 installed on a Windows Server 2003, 64-bit machine, receives the following error:

Product Line

TAC I/A Series

Environment

WorkPlace Tech Tool version 5.7.7

Windows 2003 Server, 32 bit or 64-bit

Windows 2008 Server, 32 bit or 64 bit (multiple processors)

Cause

WorkPlace Tech Tool (WPT) is not supported on computers with Windows Server operating systems, nor on computers with 64-bit operating systems.

Resolution

Install on an approved hardware platform, per the Installation Instructions.