New Release or Upgrade StruxureWare Building Operation Site Software

Issue

Steps to upgrade StruxureWare Building Operation Site Software or fresh install on clean computer

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation Site

Cause

New release of software over the top of existing or fresh install on clean machine.

Must you uninstall of StruxureWare Building Operation before installing the new version the database?

Resolution

Fresh Installation: SmartStruxure Web Help now has Building Operation products information for installation using installation packages.
With the installation packages you install, repair, upgrade, or reinstall Building Operation products. When upgrading or reinstalling, you can keep or remove software settings, licenses, or the Enterprise database. Follow this link to the Building Operation Help and search for Installation.

Upgrade Existing: SmartStruxure Web Help now has a Enterprise Server System Upgrade Workflow. Follow this link to the Building Operation Help and search for Enterprise Server System Upgrade Workflow.
Be sure to select your Product version

Note:
1. Check for the appropriate license. Licenses are version specific and are tied the "major version" only, so 1.x version licenses will work with any 1.x version. New StruxureWare Building Operation licenses will be needed for all sites beginning with v 2.0.
2. If upgrading from a Hotfix version and have an issue, contact PSS using the Contact tab above.