Issue
How can the information displayed in an alarm generated email message be controlled in R2?
Environment
Niagara R2 (all Version)
Cause
N/A
Resolution
What gets displayed in the body of an alarm generated email message is controlled by the AlarmFields property located in the MailRecipient Properties.
1. In WorkPlace Pro, right-click on the MailRecipient object and select Properties.
2. Select the Config tab.
3. Select the text fields to be displayed in the body of the email alarm to be sent to the MailRecipient.
4 Click Apply to save
The alarm generated email will contain only the selected text fields.