Issue
In a new installation, the ProView display (never configured previously) is powered and wired to the LON trunk back to a UNC-520.
In the station's LonWorks Service, a Find completes but the ProView display does not appear.
Environment
Niagara R2 version 529 or newer
ProView
Cause
"New" ProView displays are somewhat unpredictable when added to a Niagara R2 station for the first time.
Once it has been commissioned and programmed, its behavior improves.
Resolution
Add the appropriate shadow object from the 'distech' jar file (Ecdis210) to a container under the lonTrunk.
The programID for the ProView display is: 90:0:83:32:b:84:4:15
In the LonWorks Service - Lon Device Manager, highlight the just-added Ecdis210 object and Commission.
Use the SrvPin method to learn the neuronID (ProView display's service pin is located on the bottom to the left).
Once the commission process complete, ProView is now available for programming.