Order specification number for the IAC600 controller, MER207 version. (Additional node links).

Issue

To order the correct version of this controller.

Product Line

Satchwell MicroNet, Field Devices, Other

Environment

IAC600 Controller,

IAC 600 Controller,

MER207 Chip

Eaton Williams

BT Controller.

Cause

Ordering the incorrect version of controller will not allow the Eaton Williams scheme to operate correctly.

Resolution

To order the MER207 version of the IAC600 controller use the IAC600-S specification.

To download the Visisat 2.1 MER207 stencils, please click here.

Copy the downloaded file to your computer and unzip the file.
The files will be unzipped to a folder "Satchwell" with the mer files in the correct folder structure underneath.The files will unzipped to a folder "Satchwell" with the mer files in the correct folder structure underneath.

1        Copy the folder Satchwell including its sub folders.
2        To your computers C: drive.
3        This will put the required MER files in the correct places ready for use.

Now you can choose the stencil in VisiSat, when you need it, by selecting "open Stencil" and navigating to "C:\Satchwell\Binary\VisiSat\EN\Visio\Specials Products.vss.