Issue
When a user logs off a Continuum workstation, they would like the workstation to login itself maybe via a program as a Guest so that the systems can be viewed (Guest Mode).
Environment
Continuum Cyberstation and webClient (all versions)
Cause
Continuum is a security system, and as such, it requires a login for auditing purposes.
Resolution
There are no supported applications or features to provide auto-logins to Continuum. Continuum is a security system, and as such, it requires a login for auditing purposes.