Issue
Continuum add-on reports can be installed on the webclient PC, but can they display through a browser?
Environment
Continuum
Webclient
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Continuum Add-On Report Suite were not designed to be displayed through a browser with webclient
Resolution
Continuum Add-On Report Suite were not designed to be displayed through a browser with webclient.
The reports can be installed and accessed on the Cyberstation part of the Webclient PC itself, but they will not display through any of the browser PCs that connect to that Webclient PC.