Issue
An error pops up when editing a point in Video Administrator "The user currently logged on does not have edit rights for this object".
Environment
- Continuum
- Video Administrator
- Windows XP
- Windows Vista
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
There is an issue in earlier versions of Continuum 1.90/191 when using Video administrator that if an object was deleted from the controller and video admin is left open, you will receive the error.
Resolution
Upgrade to version 1.92 or greater which corrects this issue
Create another point or delete the original and recreate it.