Issue
Windows 7 Standalone v1.93. Logged into Windows as admin. Try to edit Continuum menu page to put in custom backgrounds and new .mnu file. Get error when going to run mode: "Access to c:\program...\userprofile\continuum.mnu was denied".
Environment
CyberStation running on Windows 7
Cause
Windows 7 has a security feature called User Account Control Settings that is designed to prevent potentially harmful programs from making changes to your computer. The default setting is Level 3 of 4. This setting may prevent the .MNU from updating.
Resolution
- Note: The windows logged on user must have administrator-level privileges to perform this change.
- Change the User Account Control Setting to Never Notify.
- Open Control Panel -> User Accounts.
- Click on Change User Account Control Settings.
- Drag the control to the lowest setting (Never Notify) and save.
- Restart Windows.