Totally remove the existing program from an ASC

Issue

Totally remove the existing program from an ASC

Product Line

TAC I/NET

Environment

  • I/NET Seven
  • All ASC Controllers

Cause

The ASC is not working correctly. How do I replace the existing program and start over with a new Database?

Resolution

  1. Perform a memory clear on the ASC. See Lessons Learned Article #5708 for detailed instructions.
  2. Reload the BIN files (UPD) to the controller. This is done by doing an ASC Update function in the I/NET editor
  3. Once the BIN files are loaded, bring the Points up to the Host PC. This is done by doing a MCI Update function in the I/NET editor