Issue
List view configured with qualifier Value = NotSet yet shows objects with a value of 0 (zero) as well.
Environment
All CXs
All i2s
All b3s
Cause
In Continuum NotSet evaluates to zero
Resolution
There is no way in Continuum to show only the objects that have a value of NotSet, in Continuum NotSet and zero are the same value so a list view with a qualifier 'Value = NotSet' will show objects with value set to zero as well as value set to NotSet.