Issue
Windows 7 Enterprise is not listed in the compatibility matrix for Continuum versions 1.93, 1.94, 1.94SP1 and 2.0x
Environment
Windows 7 Enterprise
Continuum versions 1.93, 1.94, 1.94SP1 and 2.0x
Cause
Windows 7 Enterprise is not listed in the compatibility matrix as a supported OS for Continuum versions 1.93, 1.94, 1.94SP1 and 2.0x
Resolution
All versions of Windows 7 require product activation.
Windows 7 Enterprise can only be activated with a Volume License MAK or KMS
Key if it is not activated against a local KMS server. Enterprise requires a
VL KMS/MAK out of the box or activation against a local KMS server. It can
be rearmed up to 3 times.
Windows 7 Ultimate edition activates conventionally via the internet to
Microsoft activation servers.
Unless you are in a business enterprise environment, then Windows 7
Ultimate should be your choice.
The Windows 7 Enterprise features and code are the same as Windows 7 Ultimate. Windows 7 Enterprise is supported.
Code is the same as Windows 7 Ultimate.
Windows 7 Enterprise is supported.