Replacement I/NET Controller NICAD Battery info

Issue

Replacement I/NET Controller NICAD Battery info.

Product Line

TAC I/NET

Environment

All I/NET controllers

Cause

Controller battery has failed, because the battery on the controller is over 5 years old  

Resolution

  1. The 3 pin version Battery is used for the NPR2000 and the DPU48K (MIP Board) -- part number 3/V80H-SLF (Note this battery has to be order from an outside Vendor and not Schneider Electric).
    Click here to view a PDF on this part.
  2. The 7910, 7920, 7930 7780 & 7940 use the 2 pin version -- part number 3/V80H-LPC (Note this battery has to be ordered from an outside Vendor and not Schneider Electric).
    Click here to view a PDF on this part.
  3. The battery used on the 7700, 7716, 7718, 7728, 7720, 7928, 7793, 7798B, & 7798C (and like controllers) is the Dallas/INET part number 801288-07. This also can be ordered from the Rockford order entry using 01-2100-545 (Old CSI P/N 801288-07). This battery also has an outside Vendor source from Power-Sonic P/N - PCBM-3.6
    Click here to view a PDF on this part.