Issue
Is TAC Vista webstation 5.1.X supported on Windows 7?
Environment
Windows 7
Webstation 5.1.X
Cause
Webstation works with Windows 7, but the reason why it's not officially supported is that the number of concurrent connections is limited to 10 (the same as in XP).
Resolution
Webstation is not supported on Windows 7. If/when an issue arises our advice will be to upgrade to a server (2003, 2008) as unexpected behaviour may be resolved simply by doing this.