Cannot reload Continuum controller

Issue

Getting error message when reloading a Continuum controller: "Unable to reload attributes for \\. Reload Object's Type mismatches with object's in WCU Controller. Please Reload WCU Controller."

Product Line

Andover Continuum

Environment

All Continuum controllers

Cause

The most common cause of this error message is duplicate alias names. For example, a controller object named "W Lobby" and a door object in the controller named "WLobby" (without the space) will have the same alias (WLobby).

Resolution

Rename one of the duplicate objects so that the alias is unique to the system.