Issue
The message “Error: Invalid compiled image file, please recompile and try again.” is displayed when attempting to download an application in WorkPlace Tech (WPT). The same message is displayed after the application had been recompiled. Also, the message “Unhandled exception during event” is displayed when opening an application in WorkPlace Tech.
Environment
WorkPlace Tech 5.x
Cause
The Workplace Tech application is corrupt.
Resolution
Use a backup copy of the application. The application will have to be reengineered if a backup application is not available.