Can not download application to a Xenta 401

Issue

Can not download application to a Xenta 401. The download looks fine until the file transfer should start. Then it just hangs and nothing happens.

Product Line

TAC Vista

Environment

Xenta 401

Cause

The problem is that a file transfer is already started for something else (trend logs or alarms) and only one file transfer can run at a time for each LON network.

Resolution

  1. Restart the Vista Server
  2. If that doesn't help, restart the Xentas to stop the ongoing file transfers