Issue
Updated license to add additional BACnet MSTP ports on the ENC and rebooted. After rebooting the added MSTP port could be enabled but the port settings could not be changed.
Environment
UNC 520
UNC license file shows "numberOfBACnetMSTPTrunks=2" (or 3 or 4)
Cause
Failure to reboot the UNC after enabling the BACnet MSTP port in the UNC
Resolution
Reboot the UNC after enabling the BACnet MSTP port.
The UNC's BACnet service will automatically detect any saved BACnet port configuration changes and will apply the changes immediately.