Issue
Customer wishes to shunt a motion sensor alarm during the day when the building is occupied. Does this require PE code or is there an easier way?
Environment
Continuum
Cause
Looking for an easier way than writing Plain English code to shunt a security alarm.
Resolution
Use an Alarm Point.
In this example, attach the schedule occupancy point in the Alarms tab of the InfinityInput editor for the motion sensor.
The alarm algorithm expression for the AlarmEnrollment object will be: Value = On and Point1 = Off (assuming AlarmPoint1 is used).
In this way, if the motion sensor is on and the occupancy schedule is off, the above expression is true, and the point will go into alarm.