File length beyond target limits.

Issue

Error received when compiling a large program.

Product Line

Andover Continuum

Environment

  • Windows XP
  • Cyber Station 1.8X and  1.9x
  • Master Controllers
  • Infinity Controllers

Cause

The following limitations apply to programs:

  • For Workstation or Infinity programs, the maximum text length is 32000 characters
  • For Infinet programs, the maximum text length is 16000 characters

Resolution

  1. Create smaller programs.
  2. Span across multiple programs.
  3. Remove comments as needed.