Issue
What are System Messages and how to stop them from coming into AMT.
Environment
All versions of I/NET Seven
Cause
System Messages provide information about events occurring in the system.
Resolution
A message can be generated when a point changes state, goes into alarm or even when a user logs on or off to the system. There are several things that the user needs to keep in mind. The set up and programming can be seen in https://ecobuilding.schneider-electric.com/search#keyword/TAC%20INET%20Documentation%20Error%20Corre... Chapter 3 System Messages.