EGL, EGRL, EGLL5 Temperature Sensors and Resistance Chart

Issue

Using the EGL, EGRL, EGLL5 which are obsolete

Product Line

TAC Vista

Environment

Vista

Cause

temperature/resistance data of EGRL, EGRLL, EGRL5 temperature sensors, or customer needs data to calibrate the sensors.

Resolution

EGL is replaced by the STD100-250

EGRL - STR100

EGLL  (2 thermistors) was not really replaced, as the average temp calc nowadays is done in the controller. The room version was named EGRLL.

All these are for the Vista series. Find the information on Sensors for Europe, Americas, and Asia Pacific

Click here for the temperature/resistance chart for the old EGL, EGRL, EGLL5

Click here for the original Product and Installation pdf.