Issue
Configuring a UNC 532 outstation.
Environment
BAS 2800+
UNC532
UNC 532
Modem
Ports
Cause
When configuring a UNC 532 outstation to use a modem, it may not be possible to connect a BAS 2800+ terminal as well.
Resolution
The UNC 532 has a limited port configuration as it's comms UARTS are shared, and therefore it cannot have a modem and a BAS 2800+ terminal configured together if the controller is communicating via the lan connection.
If the controller is operating as part of a network, i.e. via the lan, then channel 3 cannot be used. The screen shot below shows how the comms UARTS are shared. Please note that PL3 is Port 3 and PL4 is Port 2 in the Node configuration window.
If the UNC 532 is being used in a stand alone configuration, then the configurations below are possible.