Resetting a 7920 MIP Board

Issue

Downloading to a 7920 MIP and it freezes up and stops communicating.

Product Line

TAC I/NET

Environment

All versions of I/Net Software doing Access Control.

Cause

The software probably got corrupted during the download and needs to be cleared out to accept the latest bin file from the host.

Resolution

  1. With Power on and the board mounted on the 7920,
  2. On Pin Header J4, connect Pins 1 and 2 Together, via jumper or whatever medium available
  3. Press the Reset button