Issue
When saving a PE program that uses embedded Continuum functions such as SendEmail() , it errors when checking / compiling the program and shows the error message of "Unsupported feature".
Environment
Netcontroller (CX9xxx)
InfinetController(i1 , i2xxx)
BACnet controller (BCX, b4920, b3xxx)
Cause
This happens when using the controller specific functions such as SendEmail() in the Program object not the InfinityProgram object.
Resolution
Create a new InfinityProgram object in the controller , copy the source code and save. It will check successfully and save the program in the controller. After it is saved successfully, delete the problematic Program object from the controller.