Issue
Creating new stations in Niagara G3 for an ENC and Enterprise Network Server (ENS)
Environment
Niagara G3 (all versions)
Cause
Limited training on Niagara G3 and working with an ENC-520 in the office
Resolution
To create a station (ENC or ENS):
In Workbench, go to Tools > New Station to open the New Station Wizard.
To load a station in ENC:
- Open the Platform of the ENC
- Open Station Copier, and copy the desired station into the ENC. After the ENC re-boots, you can open the newly loaded ENC station
To start an ENS:
- Open the Platform of the Ent. Server station
- Open the Application Director
- Highlight the desired station, and click Start. When the station Status displays "Running", you can open the newly created Ent. Server station