Issue
When running a batch file to run an application located at C:\ from a Workstation program, Windows 7 attempts to run the application in the following location.
c:\progra~1\mocros~1\office14>plink.exe
Environment
- Windows 7
- CyberStation
- WebClient
- Shell
- Batch
Cause
Cannot successfully launch external application via a batch file using Plain English Shell command.
Resolution
Begin the batch file by specifying the fill path location.
For example:
---------------------------------------
CD\
plink.exe
---------------------------------------