Issue
Can the Roam IO/2 be used to create points in a controller?
Environment
Roam IO/2
Cause
Ability to create points with the Roam IO/2
Resolution
The Roam IO/2 device cannot be used to create points, but is designed to modify attributes of points that have been created by the Continuum system.