Issue
A 0-10 Vdc sensor will be wired into a MNL/MNB controller. The voltage must be dropped from 0-10 Vdc to 0-5 Vdc to interface and read properly. What's the part number for ordering the voltage divider used to achieve this task?
Environment
MNL controllers
MNB controllers
Cause
Another manufacturer's sensor designed with a 0-10 Vdc control signal.
Resolution
The part number is AD-8961-220. It is available for purchase via iPortal (http://iportal2.schneider-electric.com).
The controller analog input object would be set up as follows:
Linput= 0.909 Vdc
LScale= 0
Hinput= 4.545 Vdc
HScale= 100