Issue
There are times when random events require adding an exception for an Infinity schedule for the 2nd and 4th Thursday only
The recurrence may also be for a certain day, week, month or year.
Environment
- Continuum
- Windows XP
- Windows Vista
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
Bacnet schedules/calendars and programs like Microsoft Outlook allow scheduling for the 2nd and 4th Thursday, so it seems like this should be allowed in the Infinet schedules.
Resolution
In Infinity type schedules contained in Netcontrollers and infinet devices, there isn't a way to automatically ask the schedule to come on at a given time based on the 2nd or 4th Thursday, i.e. a recurrence of a day, week, month or year.
The specific date needs can be accessed by the yearly view and configured manually.