Troubleshooting guide for DMS-Microsmart bus communications

Issue

Troubleshooting guide for DMS-Microsmart bus communications

Product Line

TAC I/A Series

Environment

Microsmart controllers (all models installed with revision 9.x, 10.x, or 11.x firmware)

Cause

Troubleshooting guide for DMS-Microsmart bus communications

Resolution

TPA-RKFD-09-0010.00 is a checklist which provides several settings/configurations to review when faced with a communication problem at the controller level. The content was compiled from different resources, summarized, and laid out in an easy-to-use manner so as to provide a quick-reference document.