Does OPRIF 11.6 operate on a Windows 7 64-bit computer?

Issue

Customer is installing a new server computer and the host operating system is Windows 7 64-bit.  Will the current version of OPRIF (Operator Interface) version 11.6 operate properly if installed?

Product Line

TAC I/A Series

Environment

DMS

OPRIF 11.6 or PSOPRIF 11.6 or Operator Interface 11.6

Cause

Upgrade of computer hardware and unavailability of Windows XP

Resolution

OPRIF 11.6 will only operate on a Windows 7 64-bit operating system with XP mode installed.

For a compatibility chart, see Product Announcement PA-00163.