Issue
Is it possible to delay the alarm that occurs when OPC Server goes offline?
Environment
TAC Vista 5.1.X
Vista OPC server or client add-on
Cause
Due to network issues or temporary circumstances a customer may wish to delay this alarm to allow for short breaks in network communication
Resolution
It is not possible to delay this alarm, but the alarm can be filtered in Vista workstation.