Issue
The message "Could not invoke the command "New"" is displayed when attempting to right-click in the Drivers View Pane and add a BACnetNetwork. Also, the message "Cannot perform the drop" is displayed when attempting to drag and drop a BACnetNetwork driver from the Palette into the Drivers folder.
Environment
Niagara G3, Enterprise Network Sever, ENC-520, ENC-410
Cause
NA
Resolution
- Uninstall WorkBench
- Delete remaining folders and files from Niagara build directory
- Reinstall WorkBench