Issue
Workstation program functions while logged on to Continuum but stops functioning when the user logs off. The program disables with the error ''You do not have sufficient access to do the requested operation.'' being displayed in the Run Time tab of the program properties.
Environment
Continuum Cyberstation
Cause
When Continuum is logged off, the access rights of the default ACC user are used for things such as when Workstation programs run. If the ACC user has had its security settings restricted then these restrictions are applied when the correct user (who may not have these restrictions) is logged off of Continuum. This could then result in a workstations program trying to read / write or do some other action that it is not allowed to do under the current restriction.
Resolution
Modify your security restrictions on the ACC user to allow for actions that your Workstation Program is trying to perform.