Outside dimensions of the enclosure for the MNB-1000? Part Number MNB-1000-ENC.

Issue

Outside dimensions of the enclosure for the MNB-1000? Part Number MNB-1000-ENC.

Product Line

TAC I/A Series

Environment

Plant Controller, MNB-1000

Enclosure for the Plant Controller, MNB-1000-ENC

Cause

Need to determine mounting clearances.

Resolution

Outside dimensions are 12" wide x 111/4" high x 2 5/8" deep.

See the figure below, from the MNB-1000 Installation Instructions, F-27347-3. (Figure 3, p.3.)
 

Click here for a link to F-27347.