Issue
Global Object Alarms
.
****System Fault Priority 27**** on 28/09/2011 at 09:29:00
From Controller 60, Upto 4 global Objects unavailable from controller 255.
*************************************************************************************
Environment
- Sigma
- BAS
Cause
- An incorrect global object has been mistakenly entered and downloaded to the controller.
- A global object no longer exists.
- A large controller value and/or large object number appears in the alarm message but there is no reference to the controller or object in the object file.
Resolution
In the case of items 1 and 2 in the Cause section above.
- Correct the object reference.
- Coldstart the controller and ensure all files are downloaded to the controller.
- Check the alarm manager for any further alarms.
In the case of item 3 in the Cause section above.
It may be necessary to clear the node and re-node the controller as well and then follow the above procedure.