Xenta Software current versions as of 10/2012

Issue

What is the most current Xenta Software version for my hardware?

Product Line

TAC Vista

Environment

Xenta

Cause

The most current Xenta Software, listed by hardware platform.

Resolution

101-VF Expired product. Latest version SYS.PROG V1.10, APPL.PROG V1.12
102-AX 2.22
102-B SYS.PROG V1.10, APPL.PROG V1.10
HW1.11, SYS.PROG V1.21-01, APPL.PROG V1.10
102-EF SYS.PROG V1.10, APPL.PROG V1.10
HW1.11, SYS.PROG V1.21-01, APPL.PROG V1.10
102-ES SYS.PROG VV1.20-01, APPL.PROG V1.22
HW1.11, SYS.PROG V1.21-01, APPL.PROG V1.22 
102-VF SYS.PROG V1.10, APPL.PROG V1.10
HW1.11, SYS.PROG V1.21-01, APPL.PROG V1.10 
103-A
 
SYS.PROG V1.20-01, APPL.PROG V1.21
HW1.11, SYS.PROG V1.21-01, APPL.PROG V1.21 
104-A SYS.PROG V1.20-01, APPL.PROG V1.21
HW1.11, SYS.PROG V1.21-01, APPL.PROG V1.21
106 SYS.PROG V1.03-00, APPL.PROG V1.03
HW1.11, SYS.PROG V1.21-01, APPL.PROG V1.03 
110-D/24 SYS.PROG V1.00-05, APPL.PROG V1.02
HW1.11, SYS.PROG V1.21-01, APPL.PROG V1.02 
121-FC/24 V1.25-01 
121-HP/24 V1.25-01
151-D V1.00-02
HW1.11, V1.21-01
281 V3.87-02
282 V3.87-02
283 V3.87-02
301 V3.87-02
302 V3.87-02
301:C V3.87-02
302:C V3.87-02
401 V3.87-02
401:B V3.87-01
401:C V3.87-01
411 V1.05
412 V1.05
421A V1.14
422A V1.14
451A V1.14
452A V1.14
471 V1.04-01
491 V1.04
492 V1.04
511 V5.1.8-10
511-B V5.1.4-73
527 V5.1.8-10
527-NPR V5.1.8-08
555 V5.1.8-09
701 V5.1.8-38
711 V5.1.8-38
721 V5.1.8-38
731 V5.1.8-38
901 V3.87-02
911 V5.1.8-06
913 V5.1.8-10
OP V3.70