Issue
The G3 icon for "Start, All Programs, Enterprise Network Server 3.x., Install Platform Daemon" is missing. How to locate and run the file?
Environment
I/A Series G3 Workbench, all builds
Cause
The I/A Series G3 icons that were automatically installed in the pc Start menu are missing.
Resolution
1. On the drive where I/A Series G3 Niagara is installed, go to C:\niagara\niagara-3.n.nn\bin\plat.exe installdaemon.
2. Double click on the file plat.exe to run the executable file.